Expressions.String value function
            A function returning a string value
Format
{ Character substring function |
Remarks
A string function returns a string value and can be any one of the following:
- A SUBSTRING function to return a substring from another string. Refer to Character substring function for more details.
 - A text case conversion function, such as UPPER or LOWER. Refer to Fold function for more details.
 - A TRIM function to remove whitespace from a string. Refer to Trim function for more details.
 - An ELEMENT function to extract an element from a string of delimiter separated elements. Refer to Element function for more details.
 - A REPLACE function to replace part of a string. Refer to Replace function for more details.
 - A SOUNDEX function to return the SOUNDEX code for a string. Refer to Soundex function for more details.
 - A TRANSLATE function to return the application dictionary translated code for a string. Refer to Translate function for more details.
 - A SUBSTRING_REGEX function to return a substring from another string using regular expression pattern matching. Refer to Regex substring function for more details.